Hoofddorp, Netherlands: Murata will be exhibiting its innovative RFID solutions, featuring a live demonstration of the company's MAGICSTRAP® UHF tag-IC module, at CeBIT 2011 in Hannover, Germany, 1-5 March 2011. Murata is located in the AutoID/RFID Solutions Park on the AIM booth, Hall 7 Stand D10. The demonstration will show how RFID can be easily integrated into any electronics product by using MAGICSTRAP®. The exhibit will also highlight how cost can be saved and value can be created by the implementation of RFID inside components on a PCB; the core of any electronics product. Murata Business Development Manager Alexander Schmoldt will give a presentation on this topic on Wednesday, March 2nd from 16:30 – 17:00 at the Forum of the AutoID(RFID Solutions Park.
Murata will showcase the capabilities of its MAGICSTRAP® RFID tag for PCB traceability in a real SMD electronics production environment. Together with Murata's partners, the antenna company Kathrein, and the RFID solution provider RFIT Solutions, the MAGICSTRAP® will be shown as part of a complete system solution. This includes the reader hardware and the necessary middleware required to connect it to an existing IT environment. Once the MAGICSTRAP® RFID module is applied to a PCB it can be used not only for simple process control or traceability - as the UHF RFID will give enough read range, it can also serve as a means for anti-counterfeiting and supply chain management or maintenance history can be stored offline at the product and altered each time the product was maintained.
The special structure of the MAGICSTRAP® allows it also to function without any external antenna. This means the miniature module with a size of 3.2 x 2.5 x 0.55 mm can be embedded or molded into any product (e.g. in the case or housing) and serve as a hidden means for anti-counterfeiting.
MAGICSTRAP® is Murata's innovative RFID Tag-IC module solution. It can be mounted as a standard SMT component and makes efficient use of the PCB's ground plane as an antenna. The product itself will literally become the RFID tag. The wideband antenna matching circuit embedded into the MAGICSTRAP®, allows the module to work across all internationally allocated UHF RFID frequencies (860-960MHz). MAGICSTRAP® complies with EPC Global Class 1 Gen 2.
Murata will also show its range of upcoming RFID products, including RW-modules for HF and UHF, as well as new variants of MAGICSTRAP® which also include a version for the HF band.
Murata in Brief
Murata Manufacturing Co., Ltd. is a worldwide leader in the design, manufacture and sale of ceramic-based passive electronic components & solutions, communication modules and power supply modules. Murata is committed to the development of advanced electronic materials and leading edge, multi-functional, high-density modules. The company has employees and manufacturing facilities throughout the world.
For more information, visit Murata's website