Murata’s robots
Murata
Cheerleaders

Murata Cheerleaders' profile

Height
36cm
Weight
1.5kg
Age of members
Upper elementary school
Personality
Full of curiosity
Speed
30cm per second
Member Composition
10 Regulars + 2 Substitutes

A performance achieved with everyone working together! Murata Cheerleaders

Maintains their balance even if it looks like they’re about to fall! Great teamwork that allows them to steer away from each other!
Various stunts performed by the Murata Cheerleaders

POINT01
Maintains their balance even if it looks like they’re about to fall! Maintains their balance on the ball

They are capable of maintaining their center of gravity directly above the ground and ball. Also notice that they don’t lose their balance even when they move their arms. They are capable of performances that last up to about 1 hour within a 4 m to 4 m space. They can definitely continue cheering up until halftime of a soccer match.

POINT02
Great teamwork that allows them to steer away from each other! They can continue to move around while maintaining beautiful formations

Thanks to the technology that prevents them from crashing and enables them to maintain a certain distance from each other, they are capable of dancing as a group.

Q&A
Murata Cheerleaders’ secret

Q.How come they don’t crash into each other?

A.

They are capable of precisely recognizing each other’s location by receiving ultrasonic waves (sound) and infrared rays (light) emitted from the transmitter on the ultrasonic wave microphone and infrared sensor in their heads. This location information is sent to a computer which acts as team coach. Then, by receiving instructions from their coach, they can move around without crashing into each other.

Q.How are they able to maintain their balance?

A.

They do not fall over since the gyro sensors in their bellies measure their tilting, allowing them to shift their bodies in a direction which enable them to maintain their center of gravity directly above the ground and ball. This is the same principle as when balancing umbrellas or sticks on your hand.