• Company

Okayama Factory Installs One of Japan’s Largest Mega Solar Panel Systems

27/3/2020

Murata Manufacturing Co., Ltd.
Chairman of the Board and President:
Tsuneo Murata  

NewsArticleTitle

Murata Manufacturing Co., Ltd. has used a company parking lot for 1,200 cars, owned by its production subsidiary Okayama Murata Manufacturing (located in Setouchi City, Okayama Prefecture), to install one of Japan’s largest parking-lot-based mega solar systems. 

 

 

In order for society to continue growing sustainably, efforts to combat climate change, are seen as essential. The Murata Manufacturing Group is working on conducting business in a way that regards “strengthening our response to climate change” as a central task. Through the installation of this solar panel system, Murata is contributing to a reduction in local CO2 emissions.

Instead of conventional panels that generate electricity only on the surface, Murata’s solar panel system uses double-sided panels that are photosensitive on the reverse side as well, improving the electricity generation ratio per installation area. This way, electricity can be generated not only from direct sunlight hitting the panel surface, but also from light reflected by parked cars and the ground onto the back. With this system it will be possible to generate enough electricity to compensate for the electricity use of more than 600 standard households each year, which will lead to a CO2 reduction of 1,698 tons.
Okayama Murata Manufacturing Co., Ltd. is also planning the installation of additional double-sided solar panels in a parking lot for 500 cars in 2021. This is expected to increase the total system’s electricity generation by roughly 50% and further reduce CO2 emissions.

The Murata Manufacturing Group plans to keep promoting the use of renewable energy through the installation of solar power facilities at its domestic and overseas locations and will continue to implement efforts to combat climate change.

System Summary


Facility Name
Murata Manufacturing Solar Power Plant No. 1
Address
123-2 Okucho Fukumoto, Setouchi City, Okayama Prefecture
System Capacity
2,403 kW
Number of Installed Panels
8,010
Annual Electricity Generation Capacity (first-year estimate)
2,750,000 kWh
Annual CO2 Reduction (first-year estimate)
1,698 tons

 

Future Expansion Plan

Facility Name Murata Manufacturing Solar Power Plant No. 2
Address
77 Okucho Fukumoto, Setouchi City, Okayama Prefecture
System Capacity
1,299 kW
Number of Installed Panels
3,878
Annual Electricity Generation Capacity (first-year estimate)
1,160,000 kWh
Annual CO2 Reduction (first-year estimate)
719 tons
Planned Start of Electricity Generation
February 2021

 

 


Murata in Brief

Murata Manufacturing Co., Ltd. is a worldwide leader in the design, manufacture and sale of ceramic-based passive electronic components & solutions, communication modules and power supply modules. Murata is committed to the development of advanced electronic materials and leading edge, multi-functional, high-density modules. The company has employees and manufacturing facilities throughout the world.

For more information, visit Murata's website

Category and year of publication

Category


Year of publication