Semiconductive Property

サーミスタ

Traffic Control for Circuits.

Electric conductivity of semiconductor ceramics changes with variation in electric current and temperature making these ceramics useful for controlling household appliances and protecting them from overheating.

Materials having the resistance between those of insulators and conductors are called semiconductors. Some semiconductive ceramics have useful properties of increasing resistance against electric current when the temperature rises to a certain level (positive temperature coefficient). Murata was one the first to apply this property to succeed in mass production of PTC(positive temperature coefficient) thermistors for such applications as circuit protection. Murata also commercialized negative temperature coefficient thermistors, having a property of reduced resistance as the temperature rises, and widely used in temperature sensors and temperature compensators.

Let's take a look at the property of semiconductive ceramics.
Click here for the movie of other properties.

The Handling Products of MURATA