• CSR

Announcing the Development of MURATAGIRL ('09 Model)

2009-09-26

Murata Manufacturing Co., Ltd.
President/ Statutory Representative Director: Tsuneo Murata

MURATAGIRL

Overview

Murata Manufacturing Co., Ltd. has developed a unicycle-riding robot, MURATAGIRL ('09 model). MURATAGIRL ('09 model) will be demonstrated at the Murata booth during “CEATEC Japan 2009” held at Makuhari Messe, Chiba prefecture between Tuesday, October 6th and Saturday, October 10th.

Performance improvement

  • Can go around a curve (with a 75cm diameter)
  • Can ride over a balance beam (2cm wide)
  • Can ride at 15cm/sec (5cm/sec for the '08 model)

Main features of MURATAGIRL

  • Can come to a stop without falling
  • Can go forward or backward
  • Can maintain a set distance from the palm (tailgating ride)

Main Murata products used and features of MURATAGIRL

  1. Slant Detection Gyro Sensors (×2)

    Detects the slant angle. MURATA GIRL maintains her balance by arbitrarily controlling rotation of the wheel for front-to-back direction, and rotation of the fly-wheel built into her chest for side-to-side direction, controlled by signals from the gyro sensor.

  2. Gyro Sensor for direction detection (×1) 【NEW】

    Riding direction is detected through signals from the gyro sensor when riding around a curve.

  3. Ultrasonic sensor for detecting obstacles (transmitter and receiver are paired)

    Distance to the obstacle is determined by measuring the duration of time between transmission of ultrasonic and reception of ultrasonic bounced back from the obstacle.

  4. Bluetooth® communication module

    Commands and data are communicated with mobile information terminals and PCs over the 2.45GHz band.
    ※Bluetooth® is a registered trademark of the Bluetooth SIG Inc.

  5. General purpose components for electronic circuits

    Several of Murata's general-purpose electronic components including the chip monolithic ceramic capacitor to properly supply electricity, the ceramic resonator CERALOCK® to resonate the reference signal, the NTC Thermistor to detect temperature, a trimmer potentiometer to adjust characteristics dispersion in circuits, and the EMI suppression filter EMIFIL®, etc. are used in general electric circuits.

Background

Various types of robots capable of performing such roles as entertainment and security have been created recently for use in our daily lives. These robots incorporate several Murata products, including capacitors that store electricity in electronic circuits, sensors that control motion, and communication modules that exchange information. Since the robotics market is expected to experience strong growth, expansion in the demand for such electronic components is also expected.

For the purpose of introducing our excellent products and technological leadership, we used several Murata components that are geared toward the robotics market in MURATAGIRL and applied the advanced control and circuit design technologies that were nurtured at the foundation of our monozukuri.

In view of Japanese children’s declining interest in science, Murata has been using MURATAGIRL to actively create educational opportunities at schools under the corporate theme of “promoting science education as a part of Murata's CSR (Corporate Social Responsibility) activities, to demonstrate to children just how much fun science can be. Our efforts have been especially well received by children and educators.

In order to answer expectations for further advancement, we have developed MURATAGIRL ('09 model) to demonstrate our new technologies.

MURATA GIRL facts

Relationship to MURATABOY  Younger cousin on the father's side
Height 50cm
Weight 6kg
Birthday September 23rd
Zodiac sign Virgo
Place of birth Shiga prefecture
Favorite pastime Practicing riding her unicycle at the park
Dream Traveling around the world with MURATABOY
Personality Physically active but shy

무라타에 대해서

주식 회사 무라타 제작소는 기능성 세라믹을 기반으로 전자 디바이스의 연구 개발 • 생산 • 판매를 행하고 있으며, 재료부터 제품까지 일관 생산 체제를 구축하고 있습니다. 또한, 무라타 제품의 90%이상은 해외에서 판매되고 있으며, 국내외로 글로벌 회사를 전개하고 있습니다.

Category and year of publication

Category


Year of publication