Overview
Murata Manufacturing Co., Ltd.'s cycle-riding robots MURATA BOY and MURATA GIRL will appear on the event stage during Japan Pavilion's Kyoto Week at Expo 2010 Shanghai.
Details
Expo 2010 Shanghai Kyoto Week - A Kyoto Kaleidoscope: A Melody of Beauty and Wisdom -
Date |
Oct. 16 (Sat.) - Oct. 21 (Thurs.)
9: 30~22: 30
*Event stage activities are scheduled to end at 21: 00.
*It's the local time (Beijin time). |
Location |
Expo Shanghai Japan Pavilion Event Stage |
Sponsors |
Kyoto Metropolis, Kyoto City, Kyoto Chamber of Commerce and Industry |
Purpose |
By spreading information about Kyoto's culture and tourism opportunities, our goal is to increase the awareness and popularity of Kyoto in China; to provide publicity about Kyoto's industries and traditional crafts; to expand the market for Kyoto products; and to increase the number of Chinese tourists interested in visiting Kyoto.
|
Summary
As participants in the Shanghai Expo being held in Shanghai, China, our goal is to introduce the technologies of this company and the high technology of Kyoto to China and the rest of the world through performances by two robots developed by Murata: MURATA BOY, the bicycle-riding robot, and MURATA GIRL, the unicycle-riding robot.
Event Stage
Performances by MURATA BOY, the bicycle-riding robot, and MURATA GIRL, the unicycle-riding robot
Oct. 16 (Sat.) - Oct. 21 (Thurs.)
Two~three performance will be held per day for a total of 14 performances.
Performance Description
MURATA BOY
- Traverse a balance beam only 2 cm wide, the same width as the bicycle tires
- Traverse an S-shaped balance beam
- Come to a full stop without falling over
- Ride at very low speeds; backing up
MURATA GIRL
- Idles in place
- Moving forward and backward
- Following others
주식 회사 무라타 제작소는 기능성 세라믹을 기반으로 전자 디바이스의 연구 개발 • 생산 • 판매를 행하고 있으며, 재료부터 제품까지 일관 생산 체제를 구축하고 있습니다. 또한, 무라타 제품의 90%이상은 해외에서 판매되고 있으며, 국내외로 글로벌 회사를 전개하고 있습니다.