Overview
Murata Manufacturing Co., Ltd. has installed a mega solar system at our Yasu Division (Shiga Prefecture) . The system began operations and started generating electricity in April. This system is capable of generating sufficient annual electrical power to accommodate 200 or more normal households. In addition to promoting the widespread use of renewable energy and helping to alleviate the problem of local electricity shortages, we are also planning on putting the system to further good use by providing environmental study programs, etc. for elementary and junior high schools in cooperation with local authorities.
Murata Manufacturing will continue to adopt initiatives targeting energy saving and reducing the burden on the environment in order to contribute to solving the problems faced by the global environment.
Background
At Murata Manufacturing, we had been examining the use of renewable energy for some time as part of our initiatives to prevent global warming. The government has established a wide range of deregulation policies and renewable energy distribution policies in light of the halted nuclear power plants and the need to save power, resulting in a favorable environment for installing such systems, so we have now installed a mega solar system at our Yasu Division in Shiga Prefecture, which is located in the Kansai region of Japan, where demands for power saving are particularly high.
Summary
Address: |
2288 Oshinohara, Yasu City, Shiga |
Total Output: |
Approximately 1MW |
Number of Modules in Use: |
Approximately 3,900 |
Contractor: |
Sharp Corporation |
Annual Electricity Generation Capacity (Estimated) : |
914MWh/Year |
Application: |
Used for our fixed-price wholesale purchasing system |
Installation Period: |
Work started in November 2012, ending in April 2013 |
주식 회사 무라타 제작소는 기능성 세라믹을 기반으로 전자 디바이스의 연구 개발 • 생산 • 판매를 행하고 있으며, 재료부터 제품까지 일관 생산 체제를 구축하고 있습니다. 또한, 무라타 제품의 90%이상은 해외에서 판매되고 있으며, 국내외로 글로벌 회사를 전개하고 있습니다.