• Company

Installation of Mega Solar System in Tokyo Denpa Co., Ltd.'s Gunma Plant Completed

2014-03-31

Murata Manufacturing Co., Ltd.
President/Statutory Representative Director: Tsuneo Murata

Tokyo Denpa Co., Ltd.'s Gunma Plant

Overview

The installation of a mega solar system in Tokyo Denpa Co., Ltd.'s Gunma Plant (Sawa-gun, Gunma Prefecture) started in December 2013 has been completed and was cut-over to operations to generate electricity from March.
This project represents Murata's largest electricity generation system (generation capacity of 1.6MW) .

Background

Tokyo Denpa Co., Ltd. became a subsidiary of Murata Manufacturing Co., Ltd. on August 1, 2013, and to commemorate welcoming the company as a new member of the Murata family, the mega solar system (with an electricity generation capacity of 1.6MW) was installed within the grounds of the company's Gunma Plant in order to contribute to the widespread use of renewable energy and to facilitate the stable supply of energy in the Kanto Region. This system is capable of generating an amount of electricity equivalent to that consumed by approximately 540 households on an annual basis, and the electricity generated will be sold to Tokyo Electric Power Company, Incorporated and new power companies through the utilization of the Feed-in Tariff System.

We are also planning to cooperate with local authorities to make the system useful for environmental studies in elementary and junior high schools.

Combined with the renewable energy systems installed in the head office (50kW) , our Yasu Division (1MW) and Shenzhen Murata Technology Co., Ltd. (1MW) , the total capacity of solar-generated electricity now stands at 3.6MW.

We will continue adopting initiatives to ensure the widespread use of renewable energy, energy saving and reducing the burden on the environment into the future, and will create next-generation solutions for the global environment and contribute to the stable supply of electricity to the community.

Summary

Address: c/o Gunma Plant, Tokyo Denpa Co., Ltd., 430 Hakoishi, Tamamura-cho, Sawa-gun, Gunma
Total Output: Approximately 1.6MW
Number of Modules in Use: Approximately 6,700
Contractor: Sharp Corporation
Application: Used for the Feed-in Tariff System
Installation Period: Work started in December 2013, for completion in March 2014

무라타에 대해서

주식 회사 무라타 제작소는 기능성 세라믹을 기반으로 전자 디바이스의 연구 개발 • 생산 • 판매를 행하고 있으며, 재료부터 제품까지 일관 생산 체제를 구축하고 있습니다. 또한, 무라타 제품의 90%이상은 해외에서 판매되고 있으며, 국내외로 글로벌 회사를 전개하고 있습니다.

Category and year of publication

Category


Year of publication