2008-09-24
Murata Manufacturing Co., Ltd.
President/ Statutory Representative Director: Tsuneo Murata
Summary
Murata Manufacturing Co., Ltd. is presenting its products and technologies at CEATEC JAPAN 2008, the electronics and information technology trade show coming soon to Makuhari Messe in Chiba City.
Event name/period/venue
CEATEC JAPAN 2008—Digital Convergence:To a New Stage
Period |
Tuesday, September 30th to Saturday, October 4th
from 10:00 a.m. to 5:00 p.m. |
Venue |
Makuhari Messe in Chiba City |
Murata both number |
6C142 in Hall 6 |
Theme |
"Science Laboratory!" |
Overview
With the theme of "Science Laboratory," Murata is presenting its key devices in three zones:
- Communication and Sensing
- Automotive Applications
- Energy and Power
On the main stage, visitors can meet MURATA BOY and watch demonstrations of Murata devices on display in the three zones.
Main Stage
Let's Study Science with MURATA BOY!
We are presenting our cutting-edge technologies that are in the final stages of development through demonstrations. MURATA BOY will join with you to watch the show, which promises some surprises for visitors.
Communication and Sensing
Wireless solutions
Murata's wireless communication modules feature simplicity and compact size. Our multilayer substrate technology has made such modules possible, and our software technology ensures high throughput along with power savings. Also on display are devices that help reduce the size and increase the performance of mobile equipment such as antennas and RF components.
Motion sensing
Murata sensor systems incorporate signal processing, control circuits, software and a range of sensor elements that recognize their surroundings and changes in it. The exhibits will allow you to experience first-hand the Murata user interface technology that brings machines closer to man.
Key products
- UV Sensor Module:consists of elements that react to ultraviolet rays.
- Isolator: measures 2.0x2.0x1.0 mm, 56% smaller than the previous version.
Highlight demos
- WiFi module for simultaneous 2-channel high-definition image transmission
- Sensor systems offering the direct experience of user interface.
Automotive Applications
Sensing
Murata sensing technology reliably recognizes vehicle conditions and surroundings during driving, steering, and braking operations, helping improve car safety.
Highly reliable components
Basic Murata components that form the basis of automotive electronics include highly reliable products that take advantage of heat- and vibration-resistant ceramic characteristics and products that ensure higher joint reliability.
Key products
- Murata's lineup of components compatible with conductive adhesives now offers a greater variety of product types and sizes.
- 150℃-resistant components feature a greater operating temperature range.
- Despite their small size and light weight, Murata Rotary Position Sensors offer a warranty of up to 10 million rotations.
- Ionizers generate ions to eliminate static electricity.
Highlight demos and applications
- Angle detection demo using a Rotary Position Sensor
- Vectrix plug-in hybrid scooter incorporating Murata Monolithic Ceramic Capacitors (for high power)
Energy and Power
Thermal solutions
An increase in equipment performance translates into an increase in operating temperatures. Murata offers a range of thermal solutions for small equipment. In addition to space-saving thermal measures ranging from heat detection to cooling, these solutions include heat design assistance software and a broad lineup of components resistant to high operating temperatures.
Energy solutions
Murata also offers products that meet the requirements of power line designers. Our products for power supplies facilitate stabilization and power savings;DC-DC converters feature small installation spaces and high efficiency;and wireless quick battery charger systems have been downsized even further.
Key products
- Wire-wound Power Inductors accommodate high current and high inductance.
- DC-DC Converters offer a strong lineup of space-saving and efficient power supply modules.
Highlight demos
- Wireless quick battery charger system:Last year, Murata successfully introduced a new smaller model.
무라타에 대해서
주식 회사 무라타 제작소는 기능성 세라믹을 기반으로 전자 디바이스의 연구 개발 • 생산 • 판매를 행하고 있으며, 재료부터 제품까지 일관 생산 체제를 구축하고 있습니다. 또한, 무라타 제품의 90%이상은 해외에서 판매되고 있으며, 국내외로 글로벌 회사를 전개하고 있습니다.