• Events

Exhibition at 2012 AUTOMOTIVE ENGINEERING EXPOSITION

2012-05-07

Murata Manufacturing Co., Ltd.
President/ Statutory Representative Director: Tsuneo Murata

NewsArticleTitle

Overview

Murata Manufacturing Co., Ltd. will exhibit its products and technologies at the 2012 AUTOMOTIVE ENGINEERING EXPOSITION to be held at PACIFICO Yokohama.

Featured Exhibits

To improve the safety and environmental performance of a vehicle, more electronic components are installed in vehicles as electronic control and electric-powered systems become more advanced. Furthermore, in-vehicle connectivity is being spotlighted in expectation of technology that can be implemented for easy access to information using networks between vehicles and social infrastructure starting with connectivity between mobile equipment and in-vehicle equipment. In response to such market needs, Murata is offering a wide range of electronic components that stand up to the high-reliability factor required for vehicles, for example, sensors, which are a key component for safety and driving performance. Murata also proposes an in-vehicle wireless communication module that contributes to in-vehicle connectivity. At this exhibition, Murata will introduce electronic components and solutions that respond to these issues in automobile design.

Technical highlights of exhibit

Sensors

You will see a wide selection and application examples of automotive MEMS sensors manufactured by VTI Technologies, which has newly joined Murata Group.

  • Acceleration sensors
  • Gyro/accelerometer combo sensors
  • Pressure sensors

Energy-harvesting device

Murata will introduce the possibility of waste heat being utilized for the sensing function and reduction of the amount of wire harness, which is carried out on a test circuit that uses a combination of the energy-harvesting device (thermoelectric conversion device) and sensor.

Wireless communication module

Murata will introduce a Wi-Fi/Bluetooth® combo module that meets the high reliability required of automotive equipment.

Monolithic ceramic capacitor for inverter circuit

You will see an evaluation circuit to learn the method of switching over from an aluminum electrolytic capacitor to a monolithic ceramic capacitor for an inverter circuit.

Details

2012 AUTOMOTIVE ENGINEERING EXPOSITION

Dates: Wednesday, May 23 to Friday, May 25
Venue: PACIFICO Yokohama
Murata booth No. : P76

무라타에 대해서

주식 회사 무라타 제작소는 기능성 세라믹을 기반으로 전자 디바이스의 연구 개발 • 생산 • 판매를 행하고 있으며, 재료부터 제품까지 일관 생산 체제를 구축하고 있습니다. 또한, 무라타 제품의 90%이상은 해외에서 판매되고 있으며, 국내외로 글로벌 회사를 전개하고 있습니다.

Category and year of publication

Category


Year of publication