• Events

Exhibition at TECHNO-FRONTIER 2013

2013-07-03

Murata Manufacturing Co., Ltd.
President/Statutory Representative Director: Tsuneo Murata

NewsArticleTitle

Overview

Murata Manufacturing Co., Ltd. will conduct an exhibition at TECHNO-FRONTIER 2013, to be held at Tokyo Big Sight.

Details

TECHNO-FRONTIER 2013

Period: Wednesday, July 17 to Friday, July 19
Location: Tokyo Big Sight
URL: http://www.jma.or.jp/TF/en/index.html
Booth No. : 1D-116
1D-112
EMC JAPAN 2013
ENERGY HARVESTING 2013

Summary

EMC JAPAN 2013

Murata's booth at EMC JAPAN 2013 (Solutions for Electromagnetic Interference Exhibition) will introduce various solutions for applications that are now under the spotlight, such as noise suppression for Wi-Fi capable devices and wireless power transmission capable devices.

Noise solutions

  • Wi-Fi Over-The-Air (OTA) performance evaluation technology
  • Solutions for suppression of Wireless Local Area Network (WLAN) reception sensitivity
  • Noise suppression for LED lighting
  • Noise suppression for wireless power transmission
  • Noise suppression for electrical circuits of power amplifiers
  • Power Inductor Selection Tool (PIST) for designing circuits of DC-DC converters

Presentation

  • Noise suppression for LED lighting (three presentations per day)
  • Noise suppression for wireless power transmission (three presentations per day)
  • Times for presentations are as follows:
    10: 30am, 11: 30am, 1: 30pm, 2: 30pm, 3: 00pm, and 3: 30pm

ENERGY HARVESTING 2013

Murata's exhibit at ENERGY HARVESTING 2013 will introduce various energy-harvesting devices that can convert the tiny amounts of energy around us into electricity and a sensor network system that uses such energy-harvesting devices. The following demonstrations of these products will be provided at the exhibit.

Demonstrations

  • Sensor network system
    Murata will introduce an application of a sensor network system that combines energy-harvesting devices, sensors, and communication modules.
  • Self-powering wireless light control switch
    This wireless and battery-less switch turns lighting on and off with the energy generated by the pressing force using a piezoelectric power generating device.

Presentation

Murata will introduce various energy-harvesting devices (heat, light, vibration, and piezoelectric switches) .

Times for presentations are as follows:
11: 00am, 12: 00pm, 1: 00pm/2: 00pm


무라타에 대해서

주식 회사 무라타 제작소는 기능성 세라믹을 기반으로 전자 디바이스의 연구 개발 • 생산 • 판매를 행하고 있으며, 재료부터 제품까지 일관 생산 체제를 구축하고 있습니다. 또한, 무라타 제품의 90%이상은 해외에서 판매되고 있으며, 국내외로 글로벌 회사를 전개하고 있습니다.

Category and year of publication

Category


Year of publication