Overview
Murata Manufacturing Co., Ltd. will operate an exhibition booth at MEDTEC Japan 2014.
Details
MEDTEC Japan 2014
Period: |
Wednesday, April 9 to Friday, April 11 |
Location: |
Tokyo Big Sight |
URL: |
|
Booth No. : |
507 |
Summary
Murata will be introducing products such as short-distance wireless communication modules and various sensors that use wireless communication technology and sensing technology, which can be applied to implement smart medical and healthcare equipment, as key technologies at this exhibition.
Exhibition highlights
In the field of short-distance wireless communication technology, Murata will introduce the MAGICSTRAP® RFID device, which can read and write data using an I2C interface, has low power consumption, and does not require certification. Murata will also introduce an ultra-small and low-current-consumption Bluetooth® Smart module.
In relation to sensing technology, Murata will propose metal mesh devices that can easily detect very small quantities of a substance as well as a high-precision and low-current-consumption MEMS pressure (barometer) sensor.
In addition, Murata will exhibit AC-DC converters for medical equipment compliant with international safety standards. The use of these converters can contribute to the size reduction of medical equipment.
주식 회사 무라타 제작소는 기능성 세라믹을 기반으로 전자 디바이스의 연구 개발 • 생산 • 판매를 행하고 있으며, 재료부터 제품까지 일관 생산 체제를 구축하고 있습니다. 또한, 무라타 제품의 90%이상은 해외에서 판매되고 있으며, 국내외로 글로벌 회사를 전개하고 있습니다.