Overview
Murata will be exhibiting its products at TECHNO-FRONTIER.
Details
TECHNO-FRONTIER 2014
Period:
|
July 23 (Wednesday) to 25 (Friday)
|
Location:
|
Tokyo Big Site East Hall
|
URL:
|
|
Booth No. :
|
1D-112
|
Summary
EMC JAPAN 2014
Murata will present a variety of noise-reduction solutions for the latest applications.
Solutions for wireless power supplies for automotive applications
Measures will be presented for dealing with reduced reception sensitivity and increased emissions due to noise.
Solutions for UHS-II (high-speed differential signal transfer)
"Self-poisoning" is generated by even a very weak noise signal, and measures will be presented for dealing with the possible adverse effects of such “self-poisoning” on the wireless communication circuits of mobile devices.
In addition to the above, a wide variety of solutions will be presented, with the focus on automotive applications such as in-vehicle Ethernet and DC motors.
ENERGY HARVESTING 2014
A variety of energy harvesting elements capable of converting minute quantities of ambient energy into electricity will be exhibited, along with sensor networks employing such elements.
Piezoelectric power-generating devices
These battery-less switches require no wires and incorporate a piezoelectric element that turns the lights on and off by utilizing the energy generated when a button is pressed. The light switches will be featured in a demonstration along with newly developed rotary switches and slide panels.
In addition, a demonstration will show the use of solar power devices and monolithic thermoelectric conversion elements in a system combining sensors and wireless communication modules.
POWER SYSTEM JAPAN 2014
For the first time, Murata will exhibit its micro DC-DC converter products designed to help make electronic equipment more compact and highly functional.
The power inductor incorporates a multilayer ferrite substrate that makes possible an ultracompact size of 2.5 × 2.0 × 1.1mm and low noise characteristics. The product lineup includes voltage step-up- and step-down-type units as well as a range of sizes.
DESIGN SUPPORT SYSTEM 2014
Murata will exhibit its "Femtet®" CAE software for the first time at TECHNO-FRONTIER.
This finite element method analysis system covers a wide range of functions, including analysis of heat conduction, voltage, and sound waves, in addition to electrodynamic analysis of electric fields, magnetic fields, and electromagnetic waves. The software is user-friendly and provides an excellent cost-to-performance ratio. Visitors to the Murata booth will be able to try for themselves using Femtet® for analysis.
Presentations
- Presentations will be made within the booth on a variety of themes.
- Automotive wireless power supply noise-reduction solutions
- UHS-II noise-reduction solutions
- Solar power devices
- Monolithic thermoelectric conversion elements
- Piezoelectric power-generating devices
- Micro DC-DC converters
- "Femtet®" analysis simulation software
무라타에 대해서
주식 회사 무라타 제작소는 기능성 세라믹을 기반으로 전자 디바이스의 연구 개발 • 생산 • 판매를 행하고 있으며, 재료부터 제품까지 일관 생산 체제를 구축하고 있습니다. 또한, 무라타 제품의 90%이상은 해외에서 판매되고 있으며, 국내외로 글로벌 회사를 전개하고 있습니다.