Overview
Murata will participate in a joint exhibit with NTT Data Intellilink Corporation at the 7th Data Center Expo.
Details
7th Data Center Expo
Period: |
Wednesday, May 13 to Friday, May 15 |
Location: |
Tokyo Big Sight East Hall |
URL: |
|
Booth No.: |
East 32-35 |
Summary
Murata will exhibit products designed for use in various types of equipment installed in data centers. There will also be presentations in the Murata booth.
Products for use with HVDC racks
Murata will present lithium-ion battery modules that can be connected to a DC power supply providing high-efficiency power conversion or to an HVDC output. There will also be demonstrations of wireless sensor networks allowing monitoring of the environment within a data center.
- PFC* converters supporting 3-phase AC input
- DC-DC converters supporting high-voltage, direct current supply
- Lithium-ion batteries
- Wireless sensor networks for environment monitoring
* PFC: An abbreviation of power factor correction circuit, a type of circuit that improves the power factor. The power factor corresponds to the efficiency of an AC power supply. A power factor of 1 (100%) indicates the maximum current and voltage efficiency. A PFC circuit is designed to bring the power factor of a power supply closer to 1.
Presentations
Title: |
“Power Supplies, Lithium-ion Batteries, and Wireless Sensor Networks for HVDC” (provisional) |
Date and time: |
Friday, May 15; 1:00 to 1:30 p.m. |
무라타에 대해서
주식 회사 무라타 제작소는 기능성 세라믹을 기반으로 전자 디바이스의 연구 개발 • 생산 • 판매를 행하고 있으며, 재료부터 제품까지 일관 생산 체제를 구축하고 있습니다. 또한, 무라타 제품의 90%이상은 해외에서 판매되고 있으며, 국내외로 글로벌 회사를 전개하고 있습니다.