Murata Manufacturing Co., Ltd. has released the NFP0RSN_HL2 series of film-type common mode noise filters in the ultra-small 018012 size (0.45 x 0.30 mm).
Ever higher levels of image resolution are being engineered for compact mobile devices; this is giving rise to the demand for small-sized common mode noise filters that support the increasingly higher speeds of the differential interfaces used for data transfer.
To meet this demand, Murata has released a series of common mode noise filters in the ultra-small 018012 size (0.45 x 0.30 mm).
High-speed differential transmission lines (Mipi, USB 2.0, USB 3.1 Gen 1, etc.) in smartphones, mobile phones, wearable devices such as watches, and other small-size mobile devices
(*)Click for details of the NFP0QSN_HL2 series, its 025020 size counterpart.
주식 회사 무라타 제작소는 기능성 세라믹을 기반으로 전자 디바이스의 연구 개발 • 생산 • 판매를 행하고 있으며, 재료부터 제품까지 일관 생산 체제를 구축하고 있습니다. 또한, 무라타 제품의 90%이상은 해외에서 판매되고 있으며, 국내외로 글로벌 회사를 전개하고 있습니다.