Pick Up
Language
The robot is on a bicycle. It maintains its balance even when fully stopped! Performs various stunts such as climbing slopes and running on balance beams.
The robot is capable of riding a unicycle with its awesome sense of balance! She’s doing her best to catch up to MURATA BOY.
Maintain their balance even if it looks like they’re about to fall! Great teamwork that allows them to steer away from each other!
MURATA BOY
Birth of the first-generation MURATA BOY
Birth of the second-generation MURATA BOY
Successfully cleared its run on an S-shaped balance beam and a 10 cm wide slope, and was able to successfully park backwards!
Successfully cleared a run on a 2 cm wide slope!
MURATA GIRL
Birth of MURATA GIRL
Successful run around a curve and run over a balance beam bridge!
Successfully cleared its run on an S-shaped balance beam.
Murata Cheerleaders
Established the team of Murata Cheerleaders