Language
With respect to revenue for Year ended March 31, 2026, the Company expects an increase in capacitors and power supply modules for servers and in capacitors for distributors, despite a decrease in lithium-ion secondary batteries for power tools and multilayer resin substrates for smartphones. As a result, revenue for the next period is planned to be 1,960.0 billion yen, up 7.1% from the period. Looking at profits, the Company is projecting an operating profit of 380.0 billion yen, up 34.8% year on year; profit before tax of 390.0 billion yen, up 26.4% year on year; and profit attributable to owners of parent of 293.0 billion yen, up 25.3% year on year. This is due to profit-increasing factors such as gains from a higher operation rate resulting from an increase in production output and cost reduction, despite profit-decreasing factors such as a fall in product selling prices and increased fixed costs. Regarding capital expenditures, the Company plans to invest a total of 250.0bmillion yen primarily to expand productioncapacity for products whose demand is expected to grow, particularly from servers.
Disclaimer