Murata's surface mount technology has continued to evolve alongside the miniaturization of electronic components and the increasing density of module products. In the late 1970s, during the transition from through-hole devices (THD) to surface-mount devices (SMD), Murata pioneered the establishment of automated surface mount technology using tape reel supply. This initiative significantly contributed to the industry standardization and advancement of the reflow soldering process.
In the early 2000s, Murata was among the first to develop its own products compatible with lead-free solder. By providing mounting and reliability-related application support for these products, Murata also contributed to the realization and widespread adoption of lead-free solder mounting. Since then, Murata has continued to evolve by developing technologies such as fine printing for ultra-small components such as 0402M and 0201M size components, high-precision mounting, and solder joint technologies.
Moving forward, alongside pursuing advanced mounting technologies, we will focus on establishing sustainable mounting processes. This includes adopting low-environmental-impact materials, realizing energy-saving lines, and reducing waste. Furthermore, we will integrate with fine semiconductor manufacturing technologies and advance the development of new joining technologies. This will build the technological foundation to contribute to the future electronics society.