Language
She is capable of riding a unicycle with her awesome sense of balance! She’s doing her best to catch up to MURATA BOY.
She can stop on-the-spot by maintaining her balance with the help of the disk in her belly and pedal operations.
Can cross 2 cm-wide balance beams while maintaining her balance. She is capable of slowly crossing a balance beam while remaining constantly in the center.
I don't need to look behind me to run in reverse.
She uses her ultrasonic sensor to measure her distance from people or objects, following them while keeping a consistent distance.
Watch a movie of MURATA GIRL
The 2 gyro sensors on her back detect tilting of her body from both the front/back and left/right directions. She is capable of eliminating tilting to the left/right by rotating the disk on her chest and maintains her front/back balance by moving her wheel little by little.
MURATA GIRL is lively and shy at the same time. Her cheeks blush when she feels shy. Her cheeks turn blue if she fails to do something.