Rank |
Target substance group |
Prohibition |
Substances specified as Class I Specified Chemical Substance in Paragraph (2) of Article 2 of the Act on the Evaluation of Chemical Substances and Regulation of Their Manufacture, etc. |
Substances specified in Paragraph (1) of Article 16 of the Enforcement Order of the Industrial Safety and Health Act |
Specified poisons as prescribed in Paragraph (3) of Article 2 of the Poisonous and Deleterious Substances Control Act |
Substances specified in Pow 35-3 (1) , (3) , and (4) of Appended Table 2 of the Export Trade Control Order |
Substances classified as "Any use" under the Significant New Use Rules (SNUR) of the Toxic Substances Control Act (TSCA) |
Substances listed in Annexes A, B, C, and E of the Montreal Protocol on Substances that Deplete the Ozone Layer |
Substances listed in Chemical Weapons Convention Schedule 1 A and B |
Formaldehyde |
Benzene |
musk xylene (1-tert-butyl-3,5-dimethyl-2,4,6-trinitrobenzene) |
N-Phenyl-benzenamine reaction products with styrene and 2,4,4-trimethylpentene (BNST) |
2,4-Dichlorophenoxyacetic acid (2,4-D) |
Polycyclic aromatic hydrocarbons (PAH) |
Asbestos |
Specific aromatic amines (carcinogenic) |
Azo compounds emitting one of the specific carcinogenic aromatic amines (regulated only for specific use) |
Cadmium and its compounds |
Arsenic and its compounds (with some exceptions) |
Biocidal active substances as defined in EU Regulation 528/2012 |
Bromine-based flame retardants (PBBs, PBDEs) |
Beryllium and its compounds (used in ceramics) |
Chlorinated paraffins (short-chain) |
Chlorinated organic solvent |
Chlorinated flame retardant |
Cobalt chloride |
Hexavalent chromium compounds |
Dioxins and related compounds |
Inorganic cyanide compounds |
Acrylonitrile |
1,4-Dioxane |
Dimethyl fumarate (DMF) |
Perfluorooctane sulfonic acid (PFOS) and PFOS salts |
Perfluoroalkyl sulfonate (PFAS) |
Perfluorooctanoic acid (PFOA) and its salts and esters, Compound having perfluoroheptyl group. |
Fluorinated Green House Gases (PFCs, HFCs, Sulfur hexafluoride) |
Lead and its compounds (lead as subject to the RoHS Directive) |
Mercury and its compounds |
Metallic carbonyls |
Metallic nickel (only if users will be in constant contact with the substance) |
Specific organophosphorus compounds |
Nonylphenol ethoxylates (regulated only for specific use) |
Red phosphorus-based flame retardants |
Specific phthalic acid esters (BBP, DEHP, DBP, DIBP) |
Radioactive substances |
Thallium and its compounds (with some exceptions) |
Organotin compounds (3-substituted compounds, DBB, DBT, and DOT for specific applications) |
Polychlorinated biphenyls (PCBs) |
Monomethyl-tetrachlorodiphenyl methane |
Monomethyl-dichloro-diphenyl methane |
Monomethyldibromodiphenyl-methane (DBBT) |
Heavy metals used in packaging materials (Cd, Cr6+, Hg, Pb) |
Reduction / Avoidance |
Volatile Organic Compounds (VOCs) |
Ethylene glycol ether and its acetates |
Ethylene glycol ether and its acetates |
Antimony and its compounds (with some exceptions) |
Ethylbenzene |
Styrene |
Toluene |
Xylene |
Beryllium and its compounds (expect Ceramics) |
|
Arsenic and its compounds (copper foil for printed circuit boards, used in semiconductors) |
Lead and its compounds (ceramics, glass, high-temperature solders, etc. to which the RoHS Directive does not apply) |
N-methyl-2-pyrrolidone |
2,4-Dinitrotoluene |
Perchloric acid and perchlorates |
Bisphenol A |
Phthalic acid esters (except Specific phthalic acid esters) |
Samarium and its compounds |
Thallium (used in gold plating) |
Chlorine and chlorine containing compounds |
Bromine and bromine containing compounds |
Organostannic compounds |
Dioctyltin compounds (except when used in specified applications) |
Monitoring |
IEC62474 Declarable substance groups and declarable substances |
Substances listed on the Global Automotive Declarable Substance List (GADSL) |
Benzyl alcohol |
Iso butanol |
1-octanol |
Acetaldehyde |
Aliphatic and aromatic amines |
Cyclodeca-1,5,9-triene |
Cyclododecane |
1,3-Butadiene |
2-isopropyl-bicyclo[4.4.0]decane or 3-isopropyl-bicyclo[4.4.0]decane |
Alkylene glycol ether and its acetates |
1,4-Bis(isopropylamino)-9,10-anthraquinone |
Mineral spirit |
Dibenzofuran |
Dibenzyltoluene |
Diisopropylnaphthalene |
1,3,5-Trimethylbenzene |
Nitrobenzene |
Triisopropylnaphthalene |
1,3,5-tri-tert-butylbenzene |
Arsenic and its compounds (used in semiconductors) |
Barium and its compounds |
Biphenyls |
Bismuth and its compounds |
1,1-bis (tert-butyldioxy) -3,3,5-trimethylcyclohexane |
Chromium and its compounds (except Hexavalent chromium compounds) |
Boron and its compounds |
CMR substances |
Cobalt and its compounds |
Copper and its compounds |
Organocyanide compounds |
Fluorine and its compounds |
Gold and its compounds |
Dipentene dimer or its hydrogen addition compounds |
Maleic anhydride |
Magnesium and its compounds |
Nickel compounds |
Manganese and its compounds |
N,N-dicyclohexyl-1,3-benzothiazole-2-sulfenamide |
Nitric acid compounds and nitrous acid compounds |
Nonylphenol ethoxylates |
Palladium and its compounds |
Phenols |
Bisphenol A |
Phosphorus and its compounds |
Perchloric acid and perchlorates |
Selenium and its compounds |
Tantalum and its compounds |
Silver and its compounds |
Tellurium and its compounds |
Tin and its compounds |
Hydrogenated terphenyl |
Vanadium and its compounds |
Zinc and its compounds |
Substance of Very High Concern (SVHC) defined by the REACH regulation |
Substances listed in Chemical Weapons Convention Schedule 2 and 3 |
Hazardous substances of CLP Regulation |
Foaming polystyrene used in packaging materials |