Product Design Technology
Application/Solution Design Technology
(EMI Countermeasures Technology)
Application/Solution Design Technology (EMI Countermeasures Technology) icon

Application/Solution Design Technology (EMI Countermeasures Technology) icon

Summary

  • Generally, noise countermeasure technology involves referencing past cases and experience to optimize wiring and layout during the design phase, combining basic components such as filters and shields as needed. Noise reduction effects are verified using measuring instruments, and wiring and component configurations are adjusted to achieve gradual reduction. In recent years, design lead times have shortened, limiting the time available for prototyping and verification. This necessitates efficient noise countermeasures even under constrained conditions.
  • Murata's noise countermeasure technology precisely identifies noise sources, conduction paths, and radiation sources on electronic device boards. We then select optimal countermeasure components and propose designs that maximize their effectiveness.
  • Leveraging our testing environment and extensive practical experience, we perform component mounting on actual boards and verify effectiveness, enabling swift and precise responses to complex noise challenges. Furthermore, through PCB design support encompassing component placement and wiring patterns, we provide comprehensive countermeasure solutions.
  • We continue to evolve our technology for reducing the minute noise generated by electronic devices, reliably responding to changes in the market and next-generation communications environments.

Murata's Application/Solution Design Technology (EMI Countermeasures Technology)

Technical Explanation

Murata's noise countermeasure technology provides solutions that precisely estimate noise sources, conduction paths, and radiation sources, encompassing everything from proposing optimal countermeasure components to board design proposals that maximize their effectiveness.

This technology addresses both emission noise countermeasures and immunity noise countermeasures.

Emission Noise Countermeasures: Noise sources, generation mechanisms, conduction paths, and radiation sources are estimated and verified through noise distribution measurements and computer simulations.

Immunity Noise Countermeasures: Points susceptible to malfunction due to noise interference are identified. As with emission noise countermeasures, noise sources, conduction paths, radiation sources, and generation mechanisms are estimated and verified through measurement and simulation.

We then select components that maximize noise reduction while maintaining signal integrity and power supply quality in electronic circuits. Component selection utilizes design support tools like SimSurfing. Finally, we confirm noise suppression effectiveness through actual measurements, delivering highly reliable noise countermeasure solutions.

Image of emission problem
Image of immunity problem

Source of inserted image: Service Robot Noise Suppression-1(1/3)Open in New Window
Link: Details of Murata’s EMC support setupOpen in New Window
Link: Noise propagation on printed circuit boardsOpen in New Window

Technological Strengths

Murata's strength in noise countermeasure technology lies in its in-house noise testing environment and the diverse noise countermeasure techniques and methodologies developed through years of collaboration with electronics and semiconductor manufacturers, which can be applied to actual design boards.

Actual electronic device boards are highly complex. Consequently, the noise problems they generate are also becoming increasingly complex, involving noise radiation from multiple noise sources through various propagation paths. Even when implementing analysis and countermeasures based on theories such as radio wave propagation, electromagnetics, and electrical circuits, resolving noise issues remains difficult and may adversely affect signal integrity and power supply quality.

Murata leverages its extensive accumulated knowledge and technology in noise countermeasures to provide rapid and effective solutions for the noise challenges of increasingly complex design boards. Through these efforts, we will also support new applications and next-generation communication environments.

(Case example) Commercially available articulated robot. The radiation noise was measured at a distance of 3 meters between the antenna and the evaluation target.
Radiation noise mechanism (as investigated by Murata)
Radiation noise suppression proposal

Source of inserted image: Robot Emission Suppression Measures-1 (1/4)Open in New Window

Technological Advancement

As electronic devices have become more sophisticated and increasingly compact and thin, noise countermeasure technologies have evolved accordingly.

The increasing sophistication of electronic devices has led to a rise in the number of circuits installed. Simultaneously, the progress in making electronic devices smaller and thinner has driven the high-density mounting of semiconductors and peripheral circuit components on circuit boards.

In noise measurement, we have advanced the establishment of test environments and technologies that enable the measurement of minute noise. In noise countermeasures, we have also developed countermeasure technologies and components to effectively reduce minute noise.

Thus, alongside the evolution of electronic devices, we have comprehensively advanced noise countermeasure technologies, countermeasure components, and measurement technologies. To continue responding to changes in the electronics market, we will strive to further advance noise countermeasures.

Advancements in Noise Countermeasure Technology

Application examples for this technology

*Link to the product information site.

See here for related Murata technologies.

Examples of Application/Solution Design Technology Application ~Product Introduction~

Technology