Language
Murata Integrated Passive Solutions manufactures leading-edge integrated passive devices using a semiconductor process. Their silicon capacitors and custom component arrays target networking infrastructure (RF power and broadband), high reliability, medical, automotive and communications where high performance and miniaturization are required.
With its own R&D center and partnerships with well-known European research laboratories, Murata Integrated Passive Solutions has consolidated its position as an innovating company and can therefore anticipate customers’ needs.
Murata Integrated Passive Solutions is located in Caen, France, and has a headcount of 140. The site includes a wafer foundry (silicon wafer facility: 21 000 m² / clean room areas: 5000 m²). The manufacturing facility is certified ISO 9001 / 14001 / 18001 and IATF 16949 for the Automotive market.