Murata's Multilayer Ceramic Capacitors have driven technological innovation for many years and boast one of the world's leading product lineups. Their history has evolved together with a product portfolio that delivers high reliability and supports diverse applications.
In the early 1970s, Murata introduced compact, high-capacitance Multilayer Ceramic Capacitors to the market and developed product lines optimized for consumer electronics such as mobile phones and PCs. Products from this period featured high layer counts and stable capacitance characteristics, contributing significantly to the miniaturization and higher functionality of electronic devices.
In the 1990s, Murata focused on developing high-temperature, high-reliability Multilayer Ceramic Capacitors for automotive and industrial equipment. A representative example is the GCM series, which used heat-resistant high-dielectric materials to meet reliability requirements in harsh environments such as engine control units (ECUs) and automotive sensors.
In the 2000s, Murata further promoted lead-free compatibility, thinner designs, and multilayer structures. These products achieved high capacitance and low ESR despite their thin profiles and were widely adopted in high-frequency circuits for smartphones and tablets. During this period, Murata also strengthened its offering of low-loss products for communications infrastructure equipment.
In recent years, Murata has advanced the development of Multilayer Ceramic Capacitors that combine high withstand voltage, high reliability, and reduced environmental impact for IoT devices, electric vehicles, and renewable energy systems. As a result, adoption has expanded in electric vehicle power electronics and next-generation energy equipment.
Murata has also developed Multilayer Ceramic Capacitors with greatly improved high-frequency characteristics for AI- and 5G-related equipment. These products help maintain signal quality on high-speed communication boards and support the foundation of next-generation social infrastructure.
In this way, Murata's Multilayer Ceramic Capacitors have continued to meet increasingly diverse market needs, including miniaturization, higher capacitance, higher reliability, and high-frequency performance. By refining the features of each product, they have contributed to industrial development and improvements in quality of life. Looking ahead, Murata will continue accelerating environmental initiatives and new materials development while pursuing further performance improvements and a broader product lineup.