Language
Table of contents
Murata's sustainability initiatives are firmly rooted in the concept of resource circulation — maximizing the lifespan of finite resources while minimizing waste. This principle informs every stage of our operations, from product design to procurement, logistics, and end-of-life management. In 1994, Murata declared that it "not to make products that waste resources and energy". By 2003, we had achieved zero emissions (zero waste to landfill) at our domestic manufacturing sites. Today, we continue to set ambitious and measurable targets, including raising our sustainable resource utilization rate and our circulated resource recycling rate, with the ultimate goal of reaching 100% for both by 2050.
Our commitment to sustainability is deeply rooted in our company philosophy, Shaze, which emphasizes applying a scientific approach to continuously improve our operations and contributing to the development of society. Natural disasters caused by climate change are occurring with increasing frequency worldwide, making corporate environmental action an urgent priority for us. Murata has positioned the reduction of environmental impact as a central challenge in its business activities, promoting effective measures such as the RE100 declaration, renewable energy sourcing, and carbon pricing schemes.
As part of our ongoing efforts to achieve our RE100 targets and drive carbon neutrality across our supply chain, we are expanding our innovative packaging solution: Narrow-Pitch Taping. This sustainable packaging helps to reduce material consumption while also offering multiple other benefits to our customers.
Narrow-Pitch Taping, also known as Half-pitch taping, is a technique that reduces the space between components on a reel: the "pitch". By minimizing the pitch, we can fit twice the number of components onto a single reel without increasing the packaging size or weight. This simple yet effective change means that we can use less packaging material while maintaining the same product quantity, significantly reducing waste and storage space.
By applying narrow-pitch taping we can expect to see many benefits such as:
By using less packaging material per reel, we significantly reduce the consumption of paper and plastic, helping to minimize the environmental footprint of our products.
With more components packed efficiently in a single reel, the frequency of shipments decreases. This leads to reduced transportation needs and storage requirements, cutting down CO₂ emissions related to logistics.
Producing less packaging material means fewer natural resources, including water, are consumed in the manufacturing process, further supporting environmental conservation efforts.
Narrow-pitch taping reduces the number of setup operations on the customer's production line. This streamlines manufacturing processes, saving labor and increasing efficiency.
With reels containing more components, the space required for storage at customer sites is reduced, allowing for better inventory management.
One of the most striking outcomes of this initiative has been the ability to pack twice the number of pieces on a reel using the same amount of packaging material. This innovation effectively cuts the packaging weight and waste by more than half, having a significant impact on our sustainability goals. For our customers, this means less frequent reel changes, reduced downtime, and a smaller environmental footprint, all contributing to a more sustainable and cost-effective production process.
Implementing narrow-pitch taping was a team effort. It required close collaboration with our customers and partners to ensure seamless integration of this adapted packaging standard. Transitioning to narrow-pitch taping may involve updating some production parameters, but our team is fully prepared to provide the technical support and information needed for a seamless implementation. Through extensive dialogue and strong partnerships, we have already successfully implemented this packaging method with several customers.
This collaborative process has strengthened our shared commitment to sustainability as well as deepening our cooperation and mutual trust.
For one of our partners, managing production efficiency had become a daily challenge. Many reels were needed for certain items, taking up valuable warehouse space and slowing down the process.
After discussions with Murata, they decided to switch from 180 mm standard pitch reels to 330 mm narrow pitch reels. The change was quickly felt on the production floor. They were pleasantly surprised the number of reel changes dropped, and embraced the improvement. The switch not only made the work faster and smoother, but it also freed up space in the warehouse and cut down the amount of plastic waste being generated. Reduced environmental taxes were an added benefit which was a win for both efficiency and sustainability.
Another partner shared a different goal: reducing CO₂ emissions. They welcomed Murata's close collaboration on practical and innovative solutions such as narrow-pitch taping. Equipped with the information and the new reel options, they began making tangible steps towards a zero-emissions future.
Today, many of our customers are incorporating narrow-pitch reels into their sustainability initiatives which is positive proof that small changes on the production line can lead to big impacts in the journey toward a greener future.
By continually working with our partners and embracing innovative solutions like narrow-pitch taping, we are taking decisive steps towards achieving carbon neutrality and fulfilling our RE100 commitments. Together, we are building a greener, more efficient supply chain for the future. Working side by side with each of our customers, we consider it our mission to move forward toward the realization of a sustainable society and hope narrow-pitch taping will be adopted by more companies.
If your company is also seeking to balance environmental responsibility with productivity, we invite you to get in touch! One step toward change can make a world of difference.
Related Links
Introducing new technologies, initiatives, and business trends in electronics.