Overview
Murata Manufacturing Co., Ltd. will be exhibiting its products and technologies at the Monodzukuri Next ↑ 2014 Maintenance Techno Show.
Details
Monodzukuri Next ↑ 2014 Maintenance Techno Show
Period: |
Wednesday, November 12 to Friday, November 14 |
Location: |
Tokyo Big Sight West hall |
URL: |
|
Booth No.:
|
2A-29
|
Summary
Murata will exhibit a variety of sensors that can be used for monitoring in applications related to preventive safety and maintenance management of industrial machinery and infrastructure equipment. Also on exhibit will be sensor network solutions that combine sensors and wireless communication modules.
Sensors
Murata will exhibit for the first time compact rotation sensors for use in motor rotation control and rotary position detection for the magnetic gear. In addition, the industry’s first angular acceleration sensors, suitable for applications such as robot motion detection and motor rotation detection, will be featured in demonstrations.
Sensor Networks
Murata will display RFID technology that enables reading and writing of data over I
2C on RFID devices equipped with a wired I
2C interface. A logger module that works in combination with sensors that detect temperature or physical impacts to manage log data during distribution will be shown as an application example.
There will also be demonstrations of a wireless sensor network employing monolithic thermoelectric conversion elements, a type of energy-harvesting element.
무라타에 대해서
주식 회사 무라타 제작소는 기능성 세라믹을 기반으로 전자 디바이스의 연구 개발 • 생산 • 판매를 행하고 있으며, 재료부터 제품까지 일관 생산 체제를 구축하고 있습니다. 또한, 무라타 제품의 90%이상은 해외에서 판매되고 있으며, 국내외로 글로벌 회사를 전개하고 있습니다.