Overview
Murata Manufacturing Co., Ltd. will be exhibiting its products and technologies at Embedded Technology 2014.
Details
Embedded Technology 2014
Period: |
Wednesday, November 19 to Friday, November 21 |
Location: |
PACIFICO Yokohama |
URL: |
|
Booth No.: |
B-02 |
Summary
Murata will be exhibiting wireless communication modules, sensors, and wireless sensor network solutions that contribute to the realization of the “Internet of Things” (IoT).
Wireless communication solutions
Making possible applications for easily recording and managing life rhythms
Sample application
A demonstration will be presented in which Bluetooth® Smart modules and sensors utilizing wireless sensor network are combined to transfer data on the life rhythms of babies or small children to a smartphone or tablet device, on which it can easily be recorded and managed. It is anticipated that such systems will enable sharing of information on children’s life rhythms with medical facilities or between families.
Wireless communication solutions offering one-stop total support for hardware and software will be on display.
Wireless LAN smart module incorporating Java ME Embedded
Wi-Fi driver package for real-time OSes
Radio Law certification service with support for certification in Japan and overseas
Motion sensor modules
Murata will be exhibiting for the first time motion sensor modules that enable contactless motion detection within a 3D space, making them suitable for game machines and security applications.
Demonstrations will show the use of these modules in providing a contactless interface that operates similarly to a touch panel.
Also on display will be a sensor network that combines photoelectric devices that generate electricity from ambient indoor light, wireless communication modules, and sensors.
무라타에 대해서
주식 회사 무라타 제작소는 기능성 세라믹을 기반으로 전자 디바이스의 연구 개발 • 생산 • 판매를 행하고 있으며, 재료부터 제품까지 일관 생산 체제를 구축하고 있습니다. 또한, 무라타 제품의 90%이상은 해외에서 판매되고 있으며, 국내외로 글로벌 회사를 전개하고 있습니다.