Overview
Murata will exhibit its medical device-related technologies and solutions at MEDTEC Japan 2016.
Details
Period: |
Wednesday, April 20 through Friday, April 22 |
Location: |
Tokyo Big Sight |
Booth No.: |
6104, East Hall 6 |
Summary
MEDTEC Japan is Asia’s largest exhibition dedicated to medical device design and manufacturing, with approximately 35,000 visitors from the medical device industry expected to attend. Murata is targeting the healthcare/medical market as a target market in its business strategy and has developed miniaturization, communications, and sensing-related technologies and solutions that cater to the trend toward less invasive and more networked medical devices. At MEDTEC Japan 2016, Murata will present examples of these technologies and solutions to marketers and engineers in the industry.
Exhibition highlights
- Monolithic ceramic capacitors for implanted medical devices
- Crystal units
- MAGICSTRAP® RFID tag devices
- Tracking system based on the BLE mesh
- Demo units for wristband-type wearable devices
무라타에 대해서
주식 회사 무라타 제작소는 기능성 세라믹을 기반으로 전자 디바이스의 연구 개발 • 생산 • 판매를 행하고 있으며, 재료부터 제품까지 일관 생산 체제를 구축하고 있습니다. 또한, 무라타 제품의 90%이상은 해외에서 판매되고 있으며, 국내외로 글로벌 회사를 전개하고 있습니다.