Language
The robot is on a bicycle. It maintains its balance even when fully stopped! Performs stunts such as climbing slopes and running on balance beams.
The robot is capable of standing while maintaining its balance, even when stationary.He can also rise up from a leaning position and come to a stop while maintaining his balance.
He is capable of running without falling over. And he doesn't even have to look backwards.
He is capable of moving while maintaining his balance with the handlebars, just like a person riding a bicycle.
Can cross 2 cm-wide balance beams while maintaining his balance and can even climb and descend steep slopes with ease.
Witness his excellent driving technique. Watch him enter a curve while maintaining his balance.
With his ultrasonic sensor, he is capable of stopping before running into obstacles.
Watch a movie of MURATA BOY
Gyro sensors are capable of detecting the bicycle's slightest tilt. A force that recovers the tilting occurs by rotating the disk located in MURATA BOY's chest when tilting of the bicycle is detected. Repeating this enables MURATA BOY to maintain his balance and posture.
The Magic Stick has a built-in accelerometer and gyro sensor. When the stick is moved, data about its movement is sent to MURATA BOY over Wi-Fi, causing him to move his head or ride forward or backwards.