• Events

Exhibition Booth at Smart Energy Japan 2014

2014-01-15

Murata Manufacturing Co., Ltd.
President/Statutory Representative Director: Tsuneo Murata

NewsArticleTitle

Overview

Murata Manufacturing Co., Ltd. will operate an exhibition booth at Smart Energy Japan 2014.

Details

Smart Energy Japan 2014

Period: Wednesday, January 29 to Friday, January 31
Location: Tokyo Big Sight
URL: http://www.low-cf.jp/eng/index.html
Booth No. : 3F-09

Summary

A wireless sensor network operating without batteries through a combination of energy-harvesting technology that converts environmental energy into electricity and sensing technology and wireless technology will be on exhibit.

Demonstration

Photovoltaics

Temperature and humidity are detected with the energy generated by the light in the room, and the data collected is transmitted to a PC by the wireless communications module.

Thermoelectric conversion elements

Temperature and vibrations are detected with the energy generated from the heat given off by high-temperature pipes, and the data collected is transmitted to a PC by the wireless communications module.


무라타에 대해서

주식 회사 무라타 제작소는 기능성 세라믹을 기반으로 전자 디바이스의 연구 개발 • 생산 • 판매를 행하고 있으며, 재료부터 제품까지 일관 생산 체제를 구축하고 있습니다. 또한, 무라타 제품의 90%이상은 해외에서 판매되고 있으며, 국내외로 글로벌 회사를 전개하고 있습니다.

Category and year of publication

Category


Year of publication