2014-05-21
Murata Manufacturing Co., Ltd.
President/Statutory Representative Director: Tsuneo Murata
Overview
Murata will be exhibiting its products at JPCA Show 2014 ().
Details
JPCA Show 2014 (44th International Electronic Circuits Exhibition)
| Period: |
June 4 (Wednesday) to 6 (Friday) |
Location:
|
Tokyo Big Site East Hall
|
URL:
|
|
Booth No. :
|
East 5J-17
|
Summary
Murata will exhibit electronic circuit design and mounting technology as well as near-field wireless communication technology and CAE software for realizing new solutions in manufacturing and distribution processes.
MAGICSTRAP® near-field wireless communication technology
Small RF Tag
Murata will exhibit small RF tag that are the world’s smallest.
The antenna and matching circuit are integrated into a multilayer substrate configuration to achieve greater compactness than conventional RFID devices and allow mounting in applications with limited space.
In addition, data can be read at close proximity without the use of a dedicated antenna.
MAGICSTRAP® RFID device with wired I2C interface
Murata will exhibit an RFID device that supports reading and writing of data via an I2C interface.
Demonstrations will be presented of a logger module with integrated RFID device for managing log data during distribution and that incorporates sensors for detecting conditions such as temperature and mechanical impacts.
Femtet® CAE software
Murata will exhibit the company's Femtet® CAE software, which was developed in-house.
This finite element method analysis system was developed over many years through a process of incremental expansion of functions for the purpose of in-house product development. In addition to electromagnetic analysis of electric fields, magnetic fields, and electromagnetic waves, the software covers a wide area including heat conduction, voltage, and sound wave analysis. It is user-friendly and delivers an excellent cost-to-performance ratio.
Equipment will be set up at the booth to allow visitors to try out the Femtet® software for themselves in various analysis examples.
무라타에 대해서
주식 회사 무라타 제작소는 기능성 세라믹을 기반으로 전자 디바이스의 연구 개발 • 생산 • 판매를 행하고 있으며, 재료부터 제품까지 일관 생산 체제를 구축하고 있습니다. 또한, 무라타 제품의 90%이상은 해외에서 판매되고 있으며, 국내외로 글로벌 회사를 전개하고 있습니다.