The product information appearing in back issues of metamorphosis was current at the time of publication but may differ from the latest information in some cases. Please refer to the Murata product websiteOpen in New Window for the latest information on products.

Products & Markets

Ultrasonic Sensor

Ultrasonic Sensor Contributes to Advancement of Parking Assist System Features

Murata has succeeded in making smaller and more highly reliable ultrasonic sensors that are easy to mass-produce, based on its long-standing ceramic technology and ultrasonic sensor design technology.
Ultrasonic sensor technology will promote the permeation and advancement of parking assist system to capitalize on the recently surging global demands for automobiles especially in emerging markets.

A parking assist system (PAS) calculates the distance between the vehicle and an object (an obstacle or another vehicle) based on the time it takes for ultrasound emitted by a sensor reflecting from an object and coming back, and communicates the information to a driver for safe parking. As PAS permeates the automobile market, there was a potential demand for a small and highly reliable pin connection type sensor capable of automated mounting, from the viewpoints of lower assembly cost and quality assurance.

There was a limitation for downsizing pin-connector type ultrasonic sensors, since its pin connector had to be placed outside of the sensor unit via a support in order to reduce property degradation from its own vibration. Murata has succeeded in coming up with the structure to internalize this support within the sensor, making it possible to downsize the unit while maintaining characteristics equivalent with existing lead wire type sensors.

Also, introducing a flexible substrate for connecting a piezoelectric ceramic device and a pin connector inside the sensor, and automating the connecting process, stabilized the characteristics and improved reliability and productivity. Small pin-connector type ultrasonic sensors are advantageous for meeting the requirement to improve the resistance characteristics for electromagnetic noise, due to recent advancement in digital signal processing of PAS.

Lately, automakers are hard at work to introduce advanced driving assistance systems (ADAS) in automobiles. One of the features is detecting pedestrians and automobiles in blind spots for increased safety. Current PAS technology may be implemented to this feature, and its key device is an ultrasonic sensor. While PAS requires the detection distance of about 2m, ADAS will require about 10m. Murata will develop a high sensitivity ultrasonic sensor by hybridizing ceramic material technology, high-precision ceramic processing technology and high efficiency ultrasonic sensing technology to meet the market needs.

Overview of the PAS (Parking Assist System)

Overview of the PAS (Parking Assist System)

Small Pin-Connector Type Ultrasonic Sensor

Small Pin-Connector Type Ultrasonic Sensor

Directional Characteristics

Directional Characteristics

Blue lines and red lines show horizontal directivity and vertical directivity respectively.

ADAS Applications for Ultrasonic Sensors

ADAS Applications for Ultrasonic Sensors

Glossary

ADAS (Advanced Driving Assistance Systems):

ADAS is a generic name for driving assistance systems utilizing cutting-edge technologies including pedestrian detection, blind spot monitoring, staying in the lane and adaptive cruise control.