Common Technology Software Technology

Software Technology icon
Software Technology icon

Summary

  • Generally, software technology aims to provide generic functions and services, with limited ties to specific hardware.
  • Murata's software technology is designed to function as an integral part of the product, based on a deep understanding of its characteristics and operation. Furthermore, it covers a wide range of fields including embedded software, application software, cloud systems, and algorithms. Leveraging its close integration with hardware, it enables optimization of the entire system and the creation of new value.
  • The strength of Murata's software technology lies in developing software in parallel from the component development stage onward. This allows for detailed understanding of the characteristics of components affected by each operating environment and enables adjustments for optimal control. As a result, it becomes the “intelligence” that operates alongside the components, making it an indispensable part of the product.

Murata's Software technology

Technical Explanation

Murata's software technology is "intelligence that works together with components," designed to deeply understand hardware characteristics and maximize their potential.
This technology processes information in real time within the product. It supports the product's value in invisible ways, such as ensuring secure communication with external devices while providing users with a comfortable user experience.

Murata covers the following areas of software technology.

  • Embedded Software: We develop firmware that controls electronic components such as sensors and connectivity modules. Considering components' responsiveness and power consumption, it achieves millisecond-level high-speed processing and energy-saving operation.

  • Application Software: Responsible for the parts that users directly interact with, it provides data visualization and intuitive operation. It plays a role in enhancing product usability and experiential value.

  • Cloud Systems: We securely and efficiently manage and analyze data collected from IoT devices. This foundational technology supports integration with external services and product scalability.

  • Algorithms: We analyze sensor data in real time, extracting only the necessary information. Leveraging AI technology, we enable advanced processing such as prediction and pattern recognition.

These technologies do not function in isolation but are closely integrated with Murata's accumulated expertise in electronic components. As a result, they support the performance and reliability of products and systems as a whole, creating new user experiences.

The New Value Brought by Software

Technological Strengths

Murata's software technology excels in high performance and reliability due to its high affinity with our own hardware, as well as in features that enhance the user experience.

This strength is supported by cross-functional collaboration among multiple specialized teams, including design, evaluation, and quality assurance. We develop software in-house from the early stages of product development, gaining detailed understanding of component characteristics and user environments. This information is shared and coordinated with relevant internal departments to achieve optimal control. Through these efforts, the software functions as an integrated “intelligence” with the components, enhancing product performance and reliability.

In recent years, this technology has been expanded across multiple fields. Even in different markets such as automotive applications, medical devices, and IoT devices, Murata achieves its unique high reliability and optimal control, strengthening product competitiveness.

Cross-departmental collaboration supporting Murata's software technology strengths

Technological Advancement

Murata's software technology continues to evolve under the philosophy of “creating new value through the integration of hardware and software.”

About 20 years ago, we began our journey with the development of connectivity modules. Initially, the focus was on basic control software to operate the hardware, with limited functionality. However, over the past 20 years, the technology has steadily evolved and has now grown into a crucial element that enhances product value by integrating with the hardware.

In recent years, to handle the increasing volume of sensor data, we have actively introduced AI (artificial intelligence) and edge computing. This enables us to build mechanisms that process necessary information quickly and efficiently. Furthermore, the role of software has significantly expanded to include centralized data management through cloud integration, enhanced security, and flexible interoperability with third-party devices through standardization.

Moving forward, further evolution will be achieved by incorporating AI-based predictive control, advanced model-based development, and hybrid cloud-edge processing. Although this technology has a relatively short history, it is already being utilized across diverse product fields. It will continue to provide new value to society while maintaining and strengthening its core strengths.

The Evolution of Murata's Software Technology

Application examples for this technology

This technology is applied to Murata's products and their production processes, from research and development through mass production.

Examples of Software Technology Application ~Product Introduction~

Technology