Murata’s robots
MURATA GIRL

MURATA GIRL’s profile

Height
50cm
Weight
6kg
Birthday
September 23rd
Zodiac sign
Virgo
Hobby
Practicing riding her unicycle at the park
Dream for the future
Traveling around the world with MURATABOY
Personality
Physically active but shy
Place of birth
Shiga prefecture

Various stunts performed by MURATA GIRL

She is capable of riding a unicycle with her awesome sense of balance!
She’s doing her best to catch up to MURATA BOY.

POINT01
Idling stop

She can stop on-the-spot by maintaining her balance with the help of the disk in her belly and pedal operations.

POINT02
Balance beam run

Can cross 2 cm-wide balance beams while maintaining her balance.
She is capable of slowly crossing a balance beam while remaining constantly in the center.

POINT03
Riding in reverse

I don't need to look behind me to run in reverse.

POINT04
Following others

She uses her ultrasonic sensor to measure her distance from people or objects, following them while keeping a consistent distance.

Q&A
MURATA GIRL’s secret

Q.Why doesn’t she fall over?

A.Her secret lies in the back of her body.

The 2 gyro sensors on her back detect tilting of her body from both the front/back and left/right directions. She is capable of eliminating tilting to the left/right by rotating the disk on her chest and maintains her front/back balance by moving her wheel little by little.

Q.Does the color of MURATA GIRL’s cheeks change?

A.

MURATA GIRL is lively and shy at the same time.
Her cheeks blush when she feels shy.
Her cheeks turn blue if she fails to do something.