Language
The product information appearing in back issues of metamorphosis was current at the time of publication but may differ from the latest information in some cases. Please refer to the Murata product website for the latest information on products.
Automobiles have specific environment beyond general electronic equipment such as high-temperature operating environment for ECUs (Electronic Control Units) , and large electric power electronic circuits. Murata has commercialized ceramic capacitors to fulfill automobile-specific conditions in support of more advanced features and electrification of automobiles.
Automobiles should be safer, more comfortable and environment-friendly. In order to fulfill such requirements, thousands of ceramic capacitors are used per car to realize more advanced features and electronic control. Although GCM series, high reliability chip monolithic ceramic capacitors for automobiles, are guaranteed to operate up to 125°C, some electronic control circuits in engine rooms, transmissions and gearboxes are exposed to over 125°C. Murata has accommodated such automobile-specific high temperature circuit operation by commercializing GCG series guaranteed up to 150°C and capable of being bonded to a ceramic substrate using conductive glue.
Larger electric power needs to be supplied to electronic circuits due to the increased number of electronic control equipment from more advanced features in automobiles, as well as their use in electric vehicles and hybrid electric vehicles. KCM series, ceramic capacitors with metal terminals, responds to large electric power circuit needs, and is being made available for electronic circuits where only non-ceramic capacitors were formerly available. EVC series for large current applications is available for high power smoothing capacitor for electric cars' motor drive IGBT (Insulated Gate Bipolar Transistor) circuit and high power resonant circuit capacitors for non-contact recharging equipment.
EVC series capitalizes on ceramic capacitor characteristics to reduce component heat generation and makes equipment significantly smaller and low profile compared with non-ceramic capacitor models.
Large size monolithic ceramic capacitors, among electronic devices for automobiles, tend to be affected more from the expansion and contraction of a substrate caused by an extreme change of temperature, often causing a crack at the bonded section between a substrate and external electrode. Cracks for a capacitor itself caused by vibrations or mechanical impacts had to be dealt with also. Impacts to a capacitor itself were buffered by attaching an elastic metal terminal. Thermal shock and mechanical impacts were eased to realize high reliability. Mounting space was reduced by stacking two capacitors together. Products with rated voltage between 25 to 630 V are in the lineup.
These large-capacitance monolithic ceramic capacitors are used as a smoothing snubber for electric vehicle and hybrid electric vehicle motor drive inverters, as well as a resonant circuit for non-contact recharging equipment. With external dimensions at 16 x 20mm, their capacitance is approximately 25 times that of the largest-capacitance general-purpose capacitors. High-temperature resistance and high allowable ripple characteristics are realized, capitalizing on ceramic properties. The unit contributes to significant equipment downsizing compared with non-ceramic capacitors (allowable ripple current is over 20Arms) .