Murata's LC filter lineup has evolved into high-performance, highly reliable communication components by diversifying products in line with evolving communication standards and achieving compact, low-profile designs through proprietary technologies.
In 1989, leveraging material and multilayer technologies cultivated in Multilayer Ceramic Capacitors (MLCC), we developed filters for cordless phones. Subsequently, with the proliferation of mobile phones and advancing communication standards, we expanded into diplexers, couplers, baluns, and other components. In 2000, we commercialized the world's first balanced-matched filter for Bluetooth®.
As communication technology advances, demands for smaller mounting spaces and multi-band compatibility grow. We are driving miniaturization and low-profile designs while maintaining high performance through CC Co-fire technology and thin-film ceramic sheets. The size, which was 5.7mm × 5.0mm at inception, has evolved to 1.0mm × 0.5mm, while the height has decreased from 2.25mm to 0.3mm.
We adopted an LGA (Land Grid Array) terminal structure, placing external electrodes on the package bottom, reducing the distance to adjacent components and enabling narrow-pitch mounting.
Furthermore, we commercialized “Shield Robust,” which minimizes performance degradation caused by interference from the metal shield adjacent to the top of the filter. Even as the low profile of mobile phones increases component density, we provide products with stable performance.
Murata's multilayer LC filter lineup continues to respond flexibly and rapidly to the ever-evolving communications market and new technological demands.